CMP#.WIDTHT
Description
CMP#.WIDTHT sets the time duration of the output pulse generated by the setpointSetpoint is the target value that an automatic control system, for example PID controller, will aim to reach. It is used when CMP#.WIDTHTYPE for the setpoint is set to 1.
It takes two command line arguments: the first specifies the setpoint, and the second specifies the time duration.
Examples
Usage
Code
The following commands set the time widths of channel 1 setpoint 5 to 3.5 ms and channel 2 setpoint 1 to 20 ms.
--> CMP1.WIDTHTYPE 5 1
--> CMP1.WIDTHT 5 3.5
--> CMP2.WIDTHTYPE 1 1
--> CMP2.WIDTHT 1 20
Context
For more information please refer to Compare.
Versions
Action | Version | Notes |
---|---|---|
Implemented | 02-06-00-000 |
General Information
Type |
Read/Write |
Units |
ms |
Range |
0 to 1000.000 |
Default Value |
0 |
Data Type |
Float |
See Also |
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.